jQuery(document).ready(function($){ $('form').submit(function(e){ // validate for checkboxes if ( $('input[name=optIn1]:visible').length ) { if( !$('input[name=optIn1]:checked').length ) { alert('Please tick the "Marketing Opt-in" checkbox to submit.'); e.preventDefault(); return false; } } if ( $('input[name=PrivacyPolicy]:visible').length ) { if( !$('input[name=PrivacyPolicy]:checked').length ) { alert('Please agree to the privacy policy'); e.preventDefault(); return false; } } }); })
Decommissioning - tools and products to support oil and gas specifiers
Engineering Your Success
In meeting the requirement to remove, dismantle, clean and recycle disused oil rigs and pipelines as part of the decommissioning programme – scrapping 100+ platforms and plugging more than 1,800 oil wells in the process – oil and gas operators need to overcome some significant challenges.

As companies further develop their decommissioning systems and processes, they will look for ways to achieve efficiencies in key areas such as:
Supply chain efficiency
Technological capability
Ability to replicate systems and practice.

100 YEARS OF ENGINEERING

In a safety-critical industry, it’s important to work with business partners that you can trust. Parker was established 100 years ago, and has supported all sorts of engineering pioneers with highly challenging missions. From Charles Lindbergh’s first Atlantic crossing, to the Apollo moon landings, Oracle Team USA and the BLOODHOUND supersonic car team… our innovative motion control partnerships have supported amazing achievements across the globe.





What’s more, our experience of working across multiple industries (including automotive, aerospace, mining, health and life sciences and renewable energy) makes us ideally placed to suggest workable technology transfer options – and ways of saving time and money. It all helps when you’re aiming to reduce industry costs by 35 per cent.

Supply chain efficiency

Recent industry calls for greater transparency in scoping and bundling decommissioning projects begs the question, how can the oil and gas industry cut costs without cutting corners?

For larger service packages, pre-tagging assets prior to commencement of work may offer up savings without compromising safety. Once equipment has been tagged and documented using a robust asset management system, its status becomes instantly transparent – you can assign staffing hours, identify cleaning schedules, identify maintenance inspections and so on, right up to the point of disposal. That set-up would work equally well for operators or service providers.

Well abandonment and sealing is also key, since this accounts for a sizeable chunk of the decommissioning process. Operators and oilfield service companies exploring ‘one stop shop’ arrangements may find working with global manufacturing partners a useful strategy to drive down costs, especially when dealing with multiple product areas and territories. For example, Parker’s extensive portfolio covers everything from particle, coalescent and gas filtration, through to water-glycol and emulsion treatments, oil absorption and chemical hose products.

Technological capability

New and emerging technology has a significant part to play in the future of the oil and gas industry. Potential applications include:

Maintaining assets to the point of removal

Processing contaminated top-deck water and putting it back in the ocean

Providing energy storage to reduce generator dependency

Streamlining staffing after facilities have been made safe

Providing automated monitoring and alert services post-decommissioning.

Parker offers an unmatchable breadth and depth of technologies designed for use in oil and gas. Examples of relevant support areas include…

Asset monitoring – with the Oil & Gas Authority aiming to push out decommissioning as far as possible, extending asset life and increasing production efficiency will be key to successful implementation. The Parker Tracking System (PTS) will not only help operators manage assets safely and cost-effectively to the point of removal, it can also:

Reveal potential opportunities to reduce maintenance spend

Provide filter-based analysis reports on asset performance 

Offer automated alerts when scheduled work is due

Order parts from preferred suppliers at point of failure.

The powerful capabilities of PTS are ideally suited to operators providing ‘one stop shop’ or turnkey solutions to their customers.

Waste water and oil treatments – filtration equipment which enables final particulate separation and filtering, even with chemical-intensive slops water or attic oil to be taken to shore.








Replicating systems and practice

Now that the UK is being encouraged to assume world leadership status in decommissioning, it’s important that any lessons learned in the coming years are absorbed and replicated – for example, making sure that North Sea processes can be transferred to territories with less developed skills and systems.  

Parker’s global Oil and Gas team brings experience of supporting operations along the entire production continuum - land-based, offshore, upstream, midstream and downstream. These capabilities, combined with specially-designed products and a genuinely worldwide presence, make us a natural choice for supporting operations with scale.
OIL AND GAS EXPERTISE

Visit Parker’s oil and gas pages to view white papers, smart products and blog posts relating to the industry 
CONTACT PARKER

Questions, quotes or quick advice? 

Renewable energy – if you’re looking at possible platform re-use (such as energy storage or power generation) prior to decommissioning, Parker’s experience in photovoltaic (PV) and battery storage technology may be worth considering. We’ve worked on pioneering energy installations around the world, partnering some of the leading power generation companies to deliver highly-efficient projects.